Can we have multiple RDREC_Q function block triggered at the same time to read data from the profibus slave.The PRM module has one mailbox, so it is advisable to trigger only one RDREC_Q block at a given point of time.
Опубликовано для:Schneider Electric Казахстан