PM5110 - Does it comply with IEC 60068-2-6:2007, IEC 60068-2-27:2008?The IEC60068-2-6 & 2-27 requirements are covered in the PM5110 base standard IEC62052-11.
The Type test report is attached.
Опубликовано для:Schneider Electric Казахстан
ВложенияType test _ PM5XXX class 0.5S.pdf [1.77 MB]