Поиск часто задаваемых вопросов
Is there a solution for M340 to support OPC UA
Issue:
Does M340 Support OPC UA?
Product Line:
M340 PLC
Resolution:
Yes M340 Can support OPC UA with the Integration of EcoStruxure OPC UA Server Expert
https://www.se.com/ww/en/product-range-presentation/66388-ecostruxure%E2%84%A2-opc-ua-server-expert/
BMENUA0100 can only work with M580
Does M340 Support OPC UA?
Product Line:
M340 PLC
Resolution:
Yes M340 Can support OPC UA with the Integration of EcoStruxure OPC UA Server Expert
https://www.se.com/ww/en/product-range-presentation/66388-ecostruxure%E2%84%A2-opc-ua-server-expert/
BMENUA0100 can only work with M580
Опубликовано для:Schneider Electric Казахстан
Узнайте больше
Линейка:
Узнайте больше
Линейка: