Поиск часто задаваемых вопросов
How to configure a Modicon Switch for Port Based IP assignment
The Modicon switch has a feature that allows a user to serve the same IP address to any device connected to that specific port on the switch. This video will demonstrate how to specifically configure the switch when a 170ENT11001 Ethernet Communication Adapter will be connected to the port.
For example, if Port 3 on a Modicon switch MCSESM103F2CS0, is configured to serve an IP address 192.168.1.33, then any 170ENT11001 that is connected to Port 3 will be assigned that IP address.
For example, if Port 3 on a Modicon switch MCSESM103F2CS0, is configured to serve an IP address 192.168.1.33, then any 170ENT11001 that is connected to Port 3 will be assigned that IP address.
Опубликовано для:Schneider Electric Казахстан
Узнайте больше
Изделие:
Узнайте больше
Изделие: