Поиск часто задаваемых вопросов
Can you replace the Magelis HMI on the ATV6000 MV drive with the standard VW3A1111 HMI to monitor only?
Issue:
Monitor only with he standard VW3A1111 HMI on the ATV6000 MV drive.
Product Line:
ATV6000 MV Drives.
Environment:
All
Cause:
Replacing original HMI on the ATV6000 MV drive with the standard HMI.
Resolution:
No, you cannot substitute the Magelis HMI for the standard VW3A1111 HMI.
Опубликовано для:Schneider Electric Казахстан
Узнайте больше
Линейка:
Узнайте больше
Линейка: