Are the circuit breaker bus plugs, used on riser busway, different than the standard plug in units?
Issue:
Are the circuit breaker bus plugs, used on riser busway,  different than the standard plug in units?

Product Line:
Busway

Environment:
Application

Cause:
Clarification/Selection

Resolution:
The 800 amp and above Busplugs (Those with catalog numbers beginning with PTQ) need to be specified ("H" for horizontally mounted ) , or ("V"  for vertically mounted)..  The smaller amperage units (600A and below, beginning with PT) are the same as those used on horizontal runs.


CTA-ID : 2005901

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: