{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the part number for a 4000A plug-in tap box for CP2340G bus duct?
Issue:
Part number for a 4000A plug-in tap box for CP2340G bus duct.

Product Line:
Busway

Environment:
Products sold and used in the United States

Resolution:
Plug-in cable tap boxes are available at a rating of 1600A maximum. These can be installed on 4000A plug-in busway. The catalog number for these is either PTB316GH or PTB316GV depending on the mounting orientation of the busway - if the busway is mounted horizontally use the PTB316GH and if the busway is vertical, use the PTB316GV. End cable tap boxes (CF2340GETBMB) are available for use with CP2340G busway.





Schneider Electric Mexico

Explora más
Categoría:
Artículos que pueden ser útiles
Explora más
Categoría: