On a 9070 Type T or TF industrial control transformer (CPT) with more than one secondary voltage available, can more than one secondary voltages be utilized or only one?
Issue:
Can more than one secondary voltage be used in control transformers available with multiple secondary voltages?

Product Line:
Transformers

Environment:
Class 9070 Industrial control transformers

Resolution:
The capabilities of the various 9070 Type T and TF CPTs vary widely.  Some units can only have one voltage out with a given voltage in.  Others can have more than one.  Contact the Field Office or Product Marketing/Support for assistance.  If a satisfactory model is not available in the Industrial Control Transformer catalog, document # 9070CT9901, Square D has the capability of building virtually any CPT a customer may need, or may be able to offer a satisfactory alternate.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: