What are the repair parts for a QO342MQ225, series S3 load center?
Issue:
Repair parts for QO342MQ225 Load Center
Product Line:
QO 3-Phase Load Centers

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC342MQF for flush or QOC342MQS for surface
Interior Assembly - QO342M200I (The interior part number is OBSOLETE, but this is a current design load center and it is faster and less expensive to obtain the complete load center catalog number and change out interiors since they would be the exact same)
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QDL32225
Main Circuit Breaker Connecting Strap - 4055901903 (3 required)
Main Circuit Breaker Connecting Strap Mounting Keps Nut - 2342702001 (3 required)
Indoor Cover Mounting Screw - 4020513002K (6 required)
Indoor Cover Door Hinge - 4028356450K (3 required)
Door Latch Kit - 4020284450K

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: