What is the part number for the Model 98A temperature controller only?

Issue:
What is the catalog number for replacement of Model 98A temperature controller and the Thermo couple wire?

Product Line:
Transformer

Environment:
Medium Voltage Transformer

Resolution:
The controller only with no hardware and temperature probes respectively are part number 2480600850 and 43500-122-73. A Serial , or Factory Order number from the transformer's Nameplate would be helpful so the Factory can set the original temperature range before shipping. If none is available, the Controller will be set to the most conservative temperature range. The Thermo couple wire (43500-122-73) is sold in 60ft lengths, which are normally cut to (3) 20 ft lengths.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: