I have an HCM3691-6M interior, and want to change the main breaker to an 800A instead of 600A. Is it ok to do this?

Issue:
Will the HCM3691-6M interior accept a 800A main breaker instead of 600A?

Product Line:
I-line

Environment:
Installation

Resolution:
No. Per Peru Tag, the 600A interior is only rated for 600A, it is not the same interior as an HCM3691-8M. Therefore, though an MAP36800 would fit, it would not be acceptable.


CTA-ID : 2010392

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: