What is the maximum height for a lifting truck table used to remove metal-clad VR breakers?

Issue:
Maximum height for a lifting truck table used to remove metal-clad VR breakers.  Can it be used to remove VT`s and CPT`s drawers?

Product Line:
INMVE - MV EQUIPMENT, AIS - ANSI Withdraw

Environment:
Products sold in North America

Resolution:
The maximum height of the breaker lifting truck table used to remove metal-clad VR breaker is 66 inches.  It is not made to remove VTs and CPTs drawers.


Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: