What is the width of the Transiton section between MotorPact and Metalclad?

Issue:
Is there a transition section for connecting Masterclad and Metalclad Medium voltage Switchgear?

Product Line:
INMVE - MV EQUIPMENT

Environment:
Product Features

Resolution:
A Nema 1 transition section is available and can be used to connect between Motorpact and Metalclad switchgear, it is 14.75 inches wide.


Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: