{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Customer asks what is used for a space heater element in the H.V. switchgear?
Issue:
What product is used for the space heater element in the medium voltage switchgear?

Product Line:
Switchgear.

Environment:
Products sold in the United States.

Cause:
Product features

Resolution:
The heaters vary from product to product. HVL, HVL/cc, Visi/Vac, Metalclad. They may also vary by available control voltage and with or without guards.

The standard heater at this time for Metalclad for 120V applications with guards is the Heatrex 565074. This is a 500W 240V heater which is run at 120V. The Square D part number is 46028-126-01. There are 4 heaters per vertical section.


Schneider Electric Mexico

Explora más
Categoría:
Artículos que pueden ser útiles
Explora más
Categoría: