Is a three phase MPZ available with a 480 primary and 120/240 secondary as a special?
Issue:
Is a three phase MPZ available with a 480 primary and 120/240 secondary as a special?

Product Line:
Transformers.

Environment:
Products sold in the United States.

Cause:
Product availability.

Resolution:
No we do not build the MPZ with a center tap. The solution would be to use a single phase 240 to 120/240 transformer to feed the single phase 120v loads.


CTA-ID : 2014502

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: