Buscar Preguntas Frecuentes
Can NF panelboards and EDB, EGB, EJB circuit breakers be used for voltages other than 480Y/277Vac, 3P4W?
Product Line:
NF Panelboards
EDB, EGB, EJB Circuit Breakers
Environment:
Products installed in the US
Resolution:
Yes, NF panelboards and EDB, EGB, EJB breakers can be used on other voltage systems, with the exception of breakers with EPD suffix (equipment ground fault protection). The EPD module will only function on a 480Y/277V system. Following is the list of approved voltage systems
NF Panelboards
EDB, EGB, EJB Circuit Breakers
Environment:
Products installed in the US
Resolution:
Yes, NF panelboards and EDB, EGB, EJB breakers can be used on other voltage systems, with the exception of breakers with EPD suffix (equipment ground fault protection). The EPD module will only function on a 480Y/277V system. Following is the list of approved voltage systems
- 3P4W, 480Y/277Vac
- 3P4W, 208Y/120Vac (do not use EPD breakers)
- 3P3W, 240Vac Delta
- 3P3W, 240Vac Corner Grounded Delta (grounded B phase)
- 3P4W, 240/120Vac High Leg Delta (do not use EPD breakers)
- 1P3W, 120/240Vac (do not use EPD breakers)
Publicado para:Schneider Electric Mexico
Explora más
Rango:
Explora más
Rango: