{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the part number for the control terminal blocks used in the Model 6 LVMCC starter unit?
Issue:
Part number for the control terminal blocks used in the Model 6 LVMCC starter unit.

Product Line:
Motor Control Centers.

Environment:
Products sold in the United States.

Cause:
Replacement parts.

Resolution:
80420-830-51 - 4 pole 25A Pull-Apart Control Terminal Block assembly, used on Model 6 starter units (non-Compac 6)
80420-854-51 - 15 point 10A Pull-Apart Control Terminal Block assembly, used on Compac 6 starter units with a control power transformer control circuit
80420-854-50 - 15 point 10A Pull-Apart Control Terminal Block assembly, used on Compac 6 starter units with a separate source control circuit

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: