Are the Thermocouples included in the temperature monitor Model 98 (2480600151) kit for retro-fit of a Model 85A in existing Square D substation dry or cast resin Transformers?

Issue:
temperature monitor Model 98 (2480600151) for a retro-fit in existing Square D substation dry or cast resin Transformers
Product Line:
Medium voltage dry type Transformers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Thermocouples are  included, along with couplings, monitor, and all accessories required to install a new temperature monitor.


Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: