{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Can the TVS12RMU, remote monitor be used with the HWA series?
Issue:
Can the TVS12RMU, remote monitor be used with the HWA series?

Product Line:
Surge Protective Devices (SPDs)

Environment:
Maintenance

Cause:
Replacement

Resolution:
Yes, the remote monitor includes a 120 V AC to 12 V DC adapter with a six-foot power cord. Connections are made to the HWA SPD diagnostic panel with the twenty-four inch (61 cm) dry contact leads (provided). To extend the remote monitor further (up to 1,000 ft. (305 m)), use an additional length of solid or stranded 22 to 14 AWG wire (not provided).

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: