{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Can I use Square D Class 5230 trench duct installed on a plant floor that is going to be hosed down once a week?
Issue:
Square D Class 5230 trench duct able to be hosed down once a week

Product Line:
Wire Management

Environment:
Factory

Cause:
Product Features

Resolution:
This duct is gasketed. It will be water resistant but not water proof. The intent of the gasketing was to protect from incidental water such as a spilt bucket of water.
Hose down rating is not a feature that this product is rated for.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: