What information is available for key locks for the HVL switch?

Issue:
What information is available for key locks for the HVL switch?

Product Line:
Switchboards and Switchgear

Environment:
Medium Voltage Switchgear.

Cause:
Product features.

Resolution:
The standard OTM mechansim HVL switch has knockouts for 2 key locks below the switch handle and on the fuse door. There is a knockout for 1 key lock above the handle. The standard key lock is the Schneider Canada lock. All locks have 0`` bolt projection with the lock in the withdrawn position. ABB Kirk key locks are interchangeable. Schneider locks are Type VFL for the switch and Type VDL for fuse door. ABB Kirk locks are Type KFL for the switch and Type KDL for fuse door.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: