{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What is the part number for the Pushbutton control station panel used in Model 6 motor control center Starter Buckets?
Issue:
Replacement control station panel for Model 6 motor control center?

Product Line:
Model 6 Motor Control Center

Environment:
Products sold in North America

Resolution:
For the Telemecanique, IEC  22mm operators (max of 5 operators), part number is 80420-007-05
For the SquareD, 9001 NEMA 30mm operators (max of 3 operators), part number is 80420-007-06

NOTE
Part numbers for replacement panels do NOT fit the 6 inch Compact buckets.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: