{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
What lug kits are used for the primary and secondary of an EE250S3H?
Issue:
Transformer Lugs

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Many Transformers are shipped with bare terminals, and require lugs

Resolution:

If the primary is wired for 480V, use lug kit DASKP600. If the primary is wired for 240V, use lug kit DASKP1200. If the secondary is wired for 240V series connection, use lug kit DASKS1200. If the secondary is wired for 120V parallel connection, Square D/ Schneider Electric does not offer a lug kit for it. Customer must use an Ilsco or Anderson lug, etc.


Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: