Are NQ and NF panels available with 100% rated main breakers?

Article available in these languages: Spanish

Issue:
Can a 100% rated main circuit breaker be added to the NQ and NF panel boards?

Product Line:
Panelboards.

Environment:
NQ and NF

Cause:
N/A

Resolution:
NQ and NF Panelboards may be configured with a 100% rated PowerPact L Main Breaker if, the main breaker trip Ampacity does not exceed 400A, and it is installed in vented (NEMA 1 or 2) enclosure only. Not available in N3R.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: