Issue:
Are there replacement trims and deadfronts available for the obsolete NQOD30L100, NQOD30L100CU, NQOD430L100, NQOD430L100CU interiors?
Product Line:
NQOD panelboards
Environment:
NQOD30L100, NQOD30L100CU, NQOD430L100 NQOD430L100CU
Cause:
N/A
Resolution:
The following trim part numbers still available are for the single and three phase panels:
For the Single Phase NQOD30L100 or NQOD30L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL30L1.
For Three phase NQOD430L100 or NQOD430L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL430L1.
NOTE : All other Trims are obsolete and no longer available and will need to be fabricated by a 3rd Party Fabricator
Are there replacement trims and deadfronts available for the obsolete NQOD30L100, NQOD30L100CU, NQOD430L100, NQOD430L100CU interiors?
Product Line:
NQOD panelboards
Environment:
NQOD30L100, NQOD30L100CU, NQOD430L100 NQOD430L100CU
Cause:
N/A
Resolution:
The following trim part numbers still available are for the single and three phase panels:
For the Single Phase NQOD30L100 or NQOD30L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL30L1.
For Three phase NQOD430L100 or NQOD430L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL430L1.
NOTE : All other Trims are obsolete and no longer available and will need to be fabricated by a 3rd Party Fabricator
Publicado para:Schneider Electric Mexico
Issue:
Are there replacement trims and deadfronts available for the obsolete NQOD30L100, NQOD30L100CU, NQOD430L100, NQOD430L100CU interiors?
Product Line:
NQOD panelboards
Environment:
NQOD30L100, NQOD30L100CU, NQOD430L100 NQOD430L100CU
Cause:
N/A
Resolution:
The following trim part numbers still available are for the single and three phase panels:
For the Single Phase NQOD30L100 or NQOD30L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL30L1.
For Three phase NQOD430L100 or NQOD430L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL430L1.
NOTE : All other Trims are obsolete and no longer available and will need to be fabricated by a 3rd Party Fabricator
Are there replacement trims and deadfronts available for the obsolete NQOD30L100, NQOD30L100CU, NQOD430L100, NQOD430L100CU interiors?
Product Line:
NQOD panelboards
Environment:
NQOD30L100, NQOD30L100CU, NQOD430L100 NQOD430L100CU
Cause:
N/A
Resolution:
The following trim part numbers still available are for the single and three phase panels:
For the Single Phase NQOD30L100 or NQOD30L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL30L1.
For Three phase NQOD430L100 or NQOD430L100CU Interiors, only the Breaker dead front is still available as part number NQODRPL430L1.
NOTE : All other Trims are obsolete and no longer available and will need to be fabricated by a 3rd Party Fabricator
Publicado para:Schneider Electric Mexico