Can a new MCC section be added on the left or right of the Main or branch sections in a typical Model 6 Motor Control Center?
Issue:
Model 6 MCC section added on the left or right side of the Main or branch sections.

Product Line:
Motor Control Centers

Environment:
Application/Quotation

Cause:
Clarification

Resolution:
Yes, the Mdl 6 MCC horizontal thru bussing has the capability of being Spliced together from both sides of each section, which allows for additional sections to be added on left or right on Model 6 Motor Control Centers.

See attached Instruction bulletin for further installation clarification

Schneider Electric Mexico

Documentos adjuntos
Mdl 6 Instruction bulletin 80459-641-01E.pdf [4.36 MB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: