What terminations are available on the HCW8SN neutral assembly used on HCP I-Line interiors?
Issue:
Lug sizes

Product Line:
Panelboards

Environment:
I-Line

Cause:
Installation

Resolution:
Main Lug Terminals : (8) #3/0 - 750MCM AL/CU

(2) Bar A: (34) #4 - 14 AWG AL/CU (Each Bar A = 17 terminations.)
(1) Bar C: (9) #14 - 1/0 AWG AL/CU
(1) Bar D: (7) #6 - 350MCM AL/CU

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: