Can an empty bucket be ordered for a model 6 MCC?
Issue:
Empty bucket ordered for a Model 6 MCC.

Product Line:
Model 5 and Model 6 MCC

Environment:
Products sold in North America

Resolution:
Yes, but it must be done through the Product Selector tool (SE Advantage).  The bucket itself is 9.75 inches deep which is far short of the vertical bussing farther back in the section.  There is no provision for getting power from the Vertical or Horizontal bussing into the bucket. Power to compartment would need to be  facilitated via the vertical wireway troughs and openings in the empty mounting bucket.

Empty buckets come in 3 inch high increments starting at a minimum of 6 inches up to 48 inches high

Schneider Electric Mexico

Explora más
Categoría:
Artículos que pueden ser útiles
Explora más
Categoría: