How many 3-pole branch breakers can be installed in an MPZ30T2F?

Issue:
Breakers for MPZ products

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone Transformers by SquareD/Schneider Electric

Cause:
Mini Power Zone Transformers branch breaker capacity

Resolution:

The MPZ30T2F uses a 30 Circuit interior. 3 spaces are taken up by the backfed main breaker. The deadfront blocks 3 spaces across from the backed main.  The interior will accept a maximum of 8 three pole branch feeder breakers, or 12 two pole branch breakers or 24 single pole branch breakers.


Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: