What are the Standard Voltage Codes for NEMA Contractors and Starters?

Article available in these languages: Spanish

Issue:
Information on the common coil voltage codes for the NEMA Type S Contactors and starters

Product Line:
Contractors and Starters

Environment:
NEMA Type S

Resolution:
Voltages
60/50 HZ
24 Vac   -   V 01 (Must include Form S (Separate control) where 24 V coil is available on NEMA Starter 00-3 not available on NEMA 4-7)
120/110 Vac   -   V 02 Must include Form S (Separate control) on poly phase devices
208 Vac   -   V 08
240/220 Vac   -   V 03
480/440 Vac   -   V 06
600/550 Vac   -   V 07
Specify  V 99 For non-standard voltages. Check for availability.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: