What is the enclosure for a 1500 VA fused Transformer such as the 9070TF1500Dx?
Issue:
Enclosures for larger Industrial Control Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Enclosures only for smaller Industrial Control Transformers 1000VA and under

Resolution:
SquareD/Schneider Electric does not supply an enclosure for this size of Transformer. If the Transformer need to be placed in its own enclosure standard dimensions and heat loss characteristics of the CPTs can be found in SquareD/Schneider Electric Catalog 9070CT9901. This information will assist in sizing the proper enclosure.


CTA-ID : 2042205

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: