Does Square D supply the studs to mount the NQ interior into an existing back box?
Issue:
Are the mounting studs supplied by Square D to mount an NQ interior into an existing back box?

Product Line:
Square D Panelboards

Environment:
Retrofitting Panelboard Interiors to Old boxes

Cause:
Product features.

Resolution:
Existing box studs are not used in Square D Retrofit offering. The existing box studs can be removed. End users/Contractors need to attach the interior mounting rails to the back wall of the existing box with any fastening means they see fit.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: