{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Is the SDSA3650 compatible with a 120/240V single-phase application?
Issue:
Is the SDSA3650 compatible with a 120/240V single-phase application?

Product Line:
Surge Protection.

Environment:
Products sold in the United States.

Cause:
Application.

Resolution:
It's advisable to use the SDSA1175 instead of the SDSA3650 because the SDSA3650 starts clamping at 510V L-N and 1020V L-L, whereas the SDSA1175 starts clamping at 150V L-N and 300V L-L. Lower clamping voltages offer better protection. The SDSA1175 is not suitable for 1 Ø, 2-wire applications; the SDSA1175T must be used instead.


Schneider Electric Mexico

Explora más
Producto:
Rango:
Artículos que pueden ser útiles
Explora más
Producto:
Rango: