What are the replacement parts of the MPZ10S40F?

Issue:
Replacement Parts for MPZ10S40F Mini Power Zone

Product Line:
Transformers

Environment:
Mini Power Zones

Cause:
Maintenance

Resolution:
The following parts are replaceable: Panel Weldment: #39002-350-50, Dead Front: #39002-360-01, Hinged Cover: #39002-351-01, Back Plate: #39002-353-01, Panel Interior: #QON12CCL, Neutral Assembly is Integral with the Panel Interior.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: