What is the maximum 2-pole breaker size that can safeguard an SDSB80111 or SDSB1175C surge protective device?
Issue:
What is the maximum 2-pole breaker size that can safeguard an SDSB80111 or SDSB1175C surge protective device?

Product Line:
Surgelogic SPD

Environment:
Application

Cause:
Clarification

Resolution:
In order to safeguard an SDSB80111 or SDSB1175C, the setup should utilize a 15-20A rated breaker. Tandem breakers are not suitable for use with this device.


CTA-ID : 2046976

Schneider Electric Mexico

Explora más
Producto:
Artículos que pueden ser útiles
Explora más
Producto: