Issue:
Terminations available for HCW6SN
Product Line:
ILine panelboard
Environment:
ILine Solid Neutral
Resolution:
Terminations are as follows:
Main Lugs: (2) #4-600 and (4) 3/0-750 kcmil Cu or Al
Branch Lugs:
(34) #14-#4 Cu or Al
(9) #14-1/0 Cu or Al
(7) #6-350 kcmil Cu or Al
Terminations available for HCW6SN
Product Line:
ILine panelboard
Environment:
ILine Solid Neutral
Resolution:
Terminations are as follows:
Main Lugs: (2) #4-600 and (4) 3/0-750 kcmil Cu or Al
Branch Lugs:
(34) #14-#4 Cu or Al
(9) #14-1/0 Cu or Al
(7) #6-350 kcmil Cu or Al