{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Can a bus plug, such as catalog number PQ4610G, be installed upside down on Busway?
Issue:
What are the restrictions to installing a Busplug upside down on I Line Busway?

Product Line:
I Line II Busway

Environment:
Installation

Cause:
Orientation clarification

Resolution:
An I Line II  bus plug can only plug into a plug-in opening in one particular orientation. The bus plug ``hooks and swings`` from the side of the busway that is labeled ``Top``.
It can not ``hook and swing`` from the side opposite the Top (Which is the Bottom ).
busplug

Bus plugs are phase sensitive, so inverting switch can present a Phasing issue. A PQ4610G bus plug can be mounted on either the front, or the back side of the Busway. On Busway that is installed vertically, the handle of the bus plug will be on the Top on one side of the Busway. The handle will be located on the bottom when it is mounted on the opposite side of the Busway.

Schneider Electric Mexico

Documentos adjuntos
I Line II Instruction bulletin 45123-961-01.pdf [1.71 MB]
Explora más
Producto:
Artículos que pueden ser útiles
Explora más
Producto: