{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Are stick on number strips available for the breakers on I-Line panelboards?
Issue:
On I-Line panelboards are stick on number strips available for the breakers?

Product Line:
Square D panelboard

Environment:
I-Line panelboard

Cause:
Product features.

Resolution:
The I-Line panelboard series does not have specifically dedicated stick on number strips. However the NF panelboard strips may be used for this purpose. Order catalog number NF102OE numbered 1-102 odd/even (Left side numbered 1,3,5...101) or the NF102S numbered sequential (Left side numbered 1,2,3...51).

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: