Needs replacement fuse clip part number for Model 5 starter unit 30 amp fuse clips Class R

Issue:
Replacement  30 amp fuse clips Class R for Model 5 starter unit

Product Line:
Model 5 motor control centers.

Environment:
Products sold in the United States.

Cause:
Maintenance

Resolution:
Part numbers will be Line side 40555-122-50 quantity 3 and Load side 80409-424-50 quantity 1
Note this is for 30 amp class R high voltage and will only fit starter units not for branch units.


CTA-ID : 2049020

Schneider Electric Mexico

Explora más
Categoría:
Explora más
Categoría: