Is there a limitation on the amount of characters that can be used for a standard MCC unit's Bucket nameplate?

Issue:
How many characters will fit on an engraved Motor Control center (MCC) nameplate?

Product Line:
Motor Control Center

Environment:
Application

Cause:
Product features

Resolution:
The standard unit nameplate will hold up to 24 characters per line and up to 3 lines per nameplate.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: