Are dual circuit breaker branch feeder units (two circuit breakers in a single full size bucket, each with their own external operating handle) available for Model 6 motor control centers?

Issue:
Description of a dual feeder breaker for a MCC

Product Line:
Motot control Center

Environment:
Model 6 MCC

Cause:
Dual circuit breaker branch units save mounting space in a motor control center.

Resolution:
Dual circuit breaker branch units are not offered in Model 6 motor control centers, because "Compac 6" units are available instead.  Compac 6 branch feeder units require only six inches of mounting space, half the space required for standard units.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: