{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Video: How many spaces does the QOB3110VH, QOB3125VH, QOB3150VH breaker take in a NQOD, or NQ Panelboard?
Issue:
Spaces taken by the QOB3110VH, QOB3125VH, QOB3150VH breaker in a NQOD, or NQ Panelboard

Product Line:
NQOD/NQ Panelboards

Environment:
110-150A QOB VH Breakers

Resolution:
When installing the breaker, which will occupy 6 vertical pole spaces, the bolt on buss connections must be pulled out from underneath the breaker. After exposing the connections , screw them into the phase buss fingers of the interior. A 20A adjacent breaker is the largest that can be used in a NQOD Panel, whereas a 40A adjacent branch breaker is the largest for a NQ Panel. See process below:

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: