undefined undefined
{}

Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
Buscar Preguntas Frecuentes
Video: What is the maximum QO or QOB branch breaker (not sub-feed breaker) that can be installed in an NQ panelboard?

Article available in these languages: Spanish

Issue:
Highest ampacity QO or QOB branch breaker (not sub-feed breaker) that can be installed in an NQ panelboard

Product Line:
Branch breakers for distribution panelboards.

Environment:
NQ panelboards sold in North America.

Resolution:
The maximum QO branch breaker that can be installed in an NQ panel is a 2-pole 125Amp, 3-pole 100Amp. The maximum QOB branch breaker that can be installed in an NQ panel is a 2 or 3 Pole, 150Amp.

The following video demonstrates how to install 110-150A QOB VH breakers:

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: