Issue:
For example, if using a Hinged Right cover such as an NC38SHR, can the tubs be mounted next to each other?
Product Line:
NQ panelboards
Environment:
Products sold in North America
Cause:
Product Installation.
Resolution:
The boxes or cans can be installed mounted together. With any surface mount covers including the Hinged Right type, there is no need to allow for any spacing between cans.
For example, if using a Hinged Right cover such as an NC38SHR, can the tubs be mounted next to each other?
Product Line:
NQ panelboards
Environment:
Products sold in North America
Cause:
Product Installation.
Resolution:
The boxes or cans can be installed mounted together. With any surface mount covers including the Hinged Right type, there is no need to allow for any spacing between cans.
Publicado para:Schneider Electric Mexico
Issue:
For example, if using a Hinged Right cover such as an NC38SHR, can the tubs be mounted next to each other?
Product Line:
NQ panelboards
Environment:
Products sold in North America
Cause:
Product Installation.
Resolution:
The boxes or cans can be installed mounted together. With any surface mount covers including the Hinged Right type, there is no need to allow for any spacing between cans.
For example, if using a Hinged Right cover such as an NC38SHR, can the tubs be mounted next to each other?
Product Line:
NQ panelboards
Environment:
Products sold in North America
Cause:
Product Installation.
Resolution:
The boxes or cans can be installed mounted together. With any surface mount covers including the Hinged Right type, there is no need to allow for any spacing between cans.
Publicado para:Schneider Electric Mexico