Do the weather shields for the low voltage transformers come in a set of two to bring the enclosure rating to NEMA 3R?
Issue:
Do the weather shields for the low voltage transformers come in a set of two to bring the enclosure rating to NEMA 3R?

Product Line:
Low voltage transformers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, the weathershield kit consists of a set of two weathershields, one for the front ventilation opening and one for the rear ventilation opening. That is enough for one transformer


Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: