Issue:
Spacer bar (support) that needs to be ordered for the 3" and 4" in deep trench duct
Product Line:
Trench Duct/ Wireway
Environment:
Support of the 3" and 4" depth Trench Duct over 17" wide
Cause:
There is no listing for the support posts for 3 and 4 inch deep trench duct in the Digest and only the RSP60 posts are listed for 2 3/8" 3 3/8"deep Trench duct over 17" wide.
Resolution:
Z dividers are used for the 3"and 4" depth Trench duct , RSP60 support rods are not available for the extra depth Trench Duct. RZD603 P/N is for the Z partitions. They come in 5 ft length pieces, so for 10ft piece , 2 would be required.
Publicado para:Schneider Electric Mexico