Can a 2 pole breaker be installed in a new NQ panel with a B phase high leg?

Issue:
Can a 2 pole breaker be installed in a new NQ panel with a B phase high leg?

Product Line:
NQ Panelboards

Environment:
Products sold in North America

Resolution:
Yes, a 2 pole breaker can be installed into an NQ panel with a B phase high leg, if the B phase does not have a rejection screw in its connector .

240/120V 3phase, 4wire B high leg voltage systems will only affect 1 pole branch breakers plugged into the B phase.  The voltage from B phase to Neutral is 208V; normal 1 pole voltage from A/C phases is 120V.  Connecting to B phase with 2 or 3 pole breakers is fine as long as bussed B phase available for a breaker.

Schneider Electric Mexico

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: