Is the I-line Powerpact P-frame circuit breaker available in 100% rating?

Article available in these languages: Spanish

Issue:
I-Line mount P frame in 100% rating

Product Line:
I-Line Powerpact P Frame Circuit Breakers, I-Line panelboards and Switchboards

Enviroment:
Products sold in North America

Resolution:
The powerpact P frame I-Line circuit breaker is available with 100% rating up to 800A only.
For 100% rated 1000A and 1200A breakers, it is necessary to use the R frame Powerpact breaker.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: