Yes. You can move your ProWORX 32 authorization from one computer to another computer.
Follow the procedure below to transfer your ProWORX 32 single user authorization from the source PC to the target PC using removable media:
1- Launch the ProWORX 32 Authorization wizard on your source PC.
2- Select task Transfer Authorization.
3- Select option Transfer authorization from computer to disk.
4- Browse to the removable media and transfer authorization..
5- Launch the ProWORX 32 Authorization wizard on your target PC.
6- Insert the removable media that was used in the source.
7- Select option Transfer authorization from disk to computer.
8. Browse to the removable media.
Publicado para:Schneider Electric Mexico