Buscar Preguntas Frecuentes
What is the max ambient temp rating for the ATV212 drives?
Issue:
ATV212 drives maximum ambient temperature rating
Product Line:
Altivar ATV212
Environment:
All
Cause:
Temp ratings for the ATV212 drives
Resolution:
Operating temperature ratings is 14 to 104 degrees F without derating.
Storage temperature rating is -13 to 149 degrees F
If you need to operate the drive up to 140 degrees F or 60 degrees C you will need to derate the drive. See the install manual S1A53832.
Publicado para:Schneider Electric Mexico
Documentos adjuntos
Explora más
Rango:
Explora más
Rango: